Post Go back to editing

Transient issue MAX44284

Category: Hardware
Product Number: MAX44284

  I use the MAX44284. This compoents is used for measuring the current of a GaN transistors. In transient time at low temperature the measurement starts at 0.6 A even if the real current is about 1.3 A. This transient time occurs 8 seconds. Too long for our regulation loop. Besides it can affect the MTBF of the transistors. 

Anybody have solution to cancel this effect!

Thank you !

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.