Post Go back to editing

Transition trouble

Thread Summary

The user is experiencing a 10-second transient phase where the MAX44284 current measurement is significantly lower (0.3 A instead of 2.5 A) at low temperatures, affecting the regulation loop. Adding a thermal source reduced the transient time to about 1 second, but the issue persists. The user is advised to contact Analog Devices' technical support for further assistance.
AI Generated Content
Category: Hardware
Product Number: MAX44284

Bonjour,

   J'utilise ce composant pour l'asservissement de courant de transistor. 

J'ai une phase transitoire de 10 secondes ou le courant lu est plus bas que la valeur réelle 0.3 A au lieu de 2.5 A réel. 

Après ce temps transitoire, la valeur atteint la valeur réelle. 

Malheureusement, le système de régulation ne fonctionne pas correctement à cause de cette phase transitoire. Schéma identique à EVB.

Parents Reply Children
  • We try to add a RC filer at the output of the MAX44284 -> The issue is the same.

    Could it be important to have a transient time without over current and over voltage. The load is composed by lot of capacitors.

    Do you have any standar schematics ?

  • We have continued the investigation of the effect at low temperature. We saw the component do not work wee is its environement temperature is below 5 °C. The current read is 6 times lower compared to the value.

    Addition to this we added a thermal source o this component. We saw the transient time is reduced a lot. It could be about 1second compared to the 10 s in standard.

    We change the electric schematics to be closed to your datasheet's suggestion. No change of the issue.

    We have controlled the voltage on the RS+ and RS- on the component's pins. It is correct even if the voltage at the output is wrong.

    Please, may you have any advices ?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.