Post Go back to editing

Transition trouble

Thread Summary

The user is experiencing a 10-second transient phase where the MAX44284 current measurement is significantly lower (0.3 A instead of 2.5 A) at low temperatures, affecting the regulation loop. Adding a thermal source reduced the transient time to about 1 second, but the issue persists. The user is advised to contact Analog Devices' technical support for further assistance.
AI Generated Content
Category: Hardware
Product Number: MAX44284

Bonjour,

   J'utilise ce composant pour l'asservissement de courant de transistor. 

J'ai une phase transitoire de 10 secondes ou le courant lu est plus bas que la valeur réelle 0.3 A au lieu de 2.5 A réel. 

Après ce temps transitoire, la valeur atteint la valeur réelle. 

Malheureusement, le système de régulation ne fonctionne pas correctement à cause de cette phase transitoire. Schéma identique à EVB.

Parents Reply
  • Dear,

      I use the MAX44284. This compoents is used for measuring the current of a GaN transistors. In transient time at low temperature the measurement starts at 0.6 A even if the real current is about 1.3 A. This transient time occurs 8 seconds. Too long for our regulation loop. Besides it can affect the MTBF of the transistors. 

    Anybody have solution to cancel this effect!

    Thank you !

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.