Post Go back to editing

LT6375

Category: Hardware
Product Number: LT6375
I am building a circuit with lt6375. Here there is a problem about shutdown function. 
 
When I supplied the SHDN pin with 11V, there is no problem.
But when I connect shdn to gnd output goes 4.5V-5.5V. But it should goes high impedance as I see from datasheet. 
 
Can you verify it, when SHDN is GND, output goes to high impedance?
 
These are our voltage values in our circuit. 
 
6375_REF_ABC = 5.5V
6375_REF = 1.5V
Vcc2 = 11V

Edit Notes

simulation graph has been added.
[edited by: MuhammedBEKEN at 7:53 AM (GMT -5) on 25 Nov 2024]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.