In LTSpice I'm modeling a simple circuit using the AD8210. For space applications we are placing a 4.99Ω resistor in series with the VS pin. I noticed in the sim, that the VS pin will go up to 6V when supplied with 5V.
With the normally low current draw, the resistor doesn't cause a drop issue. But in this circuit I'm getting a boost beyond the circuit specs when I add this resistor. I would have expected ~10mV drop, not a 1V boost!
Is this just a spice model issue? Can anyone confirm with the real chip?
Thanks!
Aaron