The data sheet table specifications state that the slew rate of the ADHV4702 is typically 74V/μS.
How much does this vary? (I would like to know what the minimum value is.)
ADHV4702-1
Recommended for New Designs
The ADHV4702-1 is a high voltage (220 V), unity-gain stable precision operational amplifier. The ADHV4702-1 offers high input impedance with low input...
Datasheet
ADHV4702-1 on Analog.com
The data sheet table specifications state that the slew rate of the ADHV4702 is typically 74V/μS.
How much does this vary? (I would like to know what the minimum value is.)
PaulCA - Moved from Operational Amplifiers to Specialty Amplifiers. Post date updated from Thursday, August 29, 2024 4:51 AM UTC to Friday, August 30, 2024 1:22 AM UTC to reflect the move.
Hi UBOTI ,
The 74V/μs is characterized to the large output voltage of 200Vpp and this is without external input clamping diodes.
It may vary if you are using the clamping diodes and it would also vary based on the output voltage that you want.
What are your input signal characteristics?
Thanks and regards,
JE
The input signal is generated from the FPGA. I want to send a 200Vpp (100KHz) signal to the outside.
It is a sine wave. The gain can be adjusted from 1 to several times.
What is the minimum slew rate?
Hi UBOTI
In theory, the 100KHz can be covered by the 74V/us slew rate. For that frequency with a 200V amplitude, we only need about 59V/us slew rate to achieve it.
Thanks and regards,
JE
Hi UBOTI
In theory, the 100KHz can be covered by the 74V/us slew rate. For that frequency with a 200V amplitude, we only need about 59V/us slew rate to achieve it.
Thanks and regards,
JE
The datasheet says TYP:74V/μS,
but there is no minimum value.
Will the minimum value be 59V/μS or more?
(Or what is the probability that a sample below 59V/μS will be shipped?)
Hi UBOTI
In order to have a Min or Max value, it is preferred to have data to have from sample lots (which means many samples are needed). The datasheet only shows the typical values because it was done on a number of evaluation samples. The 59V/us is the ideal slew rate for your 200V and 100kHz frequency.
Thanks and regards,
JE
The calculations show that 59V/μS or more is needed.
>In order to have a Min or Max value, it is preferred to have data to have from sample lots (which means many samples are needed). The >>datasheet only shows the typical values because it was done on a number of evaluation samples.
I have been asking about the above many times.
What is the probability that a sample below 59V/μS will be shipped?