Hi,
Does the MAX9512 IC is obsolete or available, please suggest alternate for this part.
The page about MAX9512 IC does not give any information regarding it. we have selected and designed the system, now component is not available.
MAX9512
Production
The MAX9512 video filter amplifier with SmartSleep and Y/C mixer is ideal for portable media players (PMPs), portable DVD players, and set-top boxes (STBs...
Datasheet
MAX9512 on Analog.com
Hi,
Does the MAX9512 IC is obsolete or available, please suggest alternate for this part.
The page about MAX9512 IC does not give any information regarding it. we have selected and designed the system, now component is not available.
Hello satya,
Upon checking, unfortunately, MAX9512 has been obsoleted since June 28, 2023. For us to better suggest a suitable alternative for the part, may we know the following:
1. Critical specifications that you want
2. Target end application
3. Target package size
Having the above data will surely help us proceed with this. Thank you very much
Best regards,
Paul
Hi,
please find the point wise reply for your queries
1. Critical specifications that you want
R: need to merge Y/C to CVBS
2. Target end application
R: Video loop back generator
3. Target package size
R: 200Units
please also suggest the alternate for ADV7340.
One request or suggestion from my end if any part is going to obsolete then please arrange or suggest alternate part on the same product page.
BR
Satyanarayana.
Hello satya,
Please refer to the following:
1. Critical specifications that you want
R: need to merge Y/C to CVBS
- Forgive me but I don't quite get what you mean here. When I asked you about the critical specs, I was referring to the parameters that can be found on a part's data sheet, like input bias current, offset voltage, bandwidth, etc. Do you have any target specifications?
3. Target package size
R: 200Units
- What I've meant about the package size is the actual package of the IC and not the number/quantity of the IC. For example, MAX9512 is available in a Thin QFN package. Do you also have a target IC package? (SOIC? MSOP? etc.)
For ADV7340's replacement, I recommend you to ask it on the Video community because we do not support non-amplifier products on this forum. Thank you.
Best regards,
Paul
hi Paul,
1. Critical specifications that you want
R: Not so specific or critical, What Max9512 IC offers is acceptable means similar parameters
3. Target package size
R: Not so specific except BGA, similar package of Max9512 IC or any also ok.
BR,
satya
Hi satya ,
Good day. You may want to check this part: https://www.analog.com/media/en/technical-documentation/data-sheets/ada4410-6.pdf. Unfortunately, we don't have any pin-to-pin compatible for MAX49512. Let me know if there's anything we can help.
Thanks and regards,
Gilbeys
Satya,
I ran into the same issue to merge Y/C to CVBS and found the MAX9512 is no longer available. What I've found so far is NJM2274 (from Nisshinbo) and it is available at Mouser's. Haven't ordered a sample yet, but the datasheet suggests that it will do the job. See here:
www.mouser.com/.../NJM2274_E-1917180.pdf
All the best,
VK