Post Go back to editing

Differential Input Voltage

Thread Summary

The user inquires if the AD8212 can handle differential input voltages greater than 500mV, specifically 800mV, in a high-voltage application with an external PNP rated at +140V. The support engineer advises that exceeding the 500mV differential input limit could damage the AD8212 and is not recommended.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8212

Hello, 

Iam curious if the AD8212 can handle Differential Input Voltage that is greater than the Table 1 specified 500mV number? 

Note: iam using this device in high voltage operation with an external PNP rated at +140V

I am expecting a current spike that will cause they Diff voltage seen at the input pins to be ~800mV. ( iam more interested in surviving this rather than actually sensing the current) 

What happens if this is applied to the AD8212?