Post Go back to editing

LT1970 Current source mode (DC2591A)

Category: Datasheet/Specs
Product Number: LT1970A

Hi everyone,

According to the demo manual DC2591A, the EasySMU board is described as a 'programmable-voltage/programmable-current' source (see the attached image from the first page of the datasheet).

I assume this functionality is provided by the LT1970 Power Op Amp at the core of the board. However, I'm a bit unclear on how it's being used as a current source. From what I can see, the EasySMU code doesn’t appear to directly set an output current (by set, I mean force like an SMU would); it seems to only set a current limit (using the 'fltSetCommitCurrentSource()' and 'CommitCurrentSourceSetting()' functions).

I've run some simulations with LTSpice using the provided model of the Op Amp, but I haven't been able to achieve a constant current through any load.

Could someone clarify how the current source functionality is implemented ?

Thanks a lot !



Added the precision that I am doing simulations.
[edited by: PiR at 2:47 PM (GMT -4) on 18 Aug 2024]

Thread Notes

Parents Reply Children
  • To be honest, your answer doesn't directly address the question I initially asked. However, I have realized that my question was based on a misunderstanding of how voltage sources operate. I believe I have now resolved this issue.

    Initially, I thought the user needed to configure the LT1970A specifically as a current source. But this isn’t the case -- the LT1970A automatically switches from voltage source mode to current source mode when the current limit is reached (see attached image from the datasheet).

    Thank you