Post Go back to editing

AD8460 as Programmable Power Supply without Heatsink

Category: Datasheet/Specs
Product Number: AD8460

I'd like to use the AD8460 as a simple power supply no AWG capability needed:

Power In: (+/-24V) or (+42V and -24V)

Power Out: +/-16V <50mA

SOA:  It seems like I would be well within the SOA for operation without a heat sink.

SPI Communication:  Is there an option to daisy chain devices using the SPI interface?

Thank you,

Tony

Thread Notes