We need to monitor the current through a Shunt resistance of 40mOhm.
For the diagnostic purpose, we are planning to keep 1K ohm resistor in series between the IN+ & IN- pins and the shunt resistor.
So now the questions are,
1. Is it allowed to have 1K ohm resistance in front of IN+ & IN- pins of MAX49925 device?
2. What is the functional impact of having high input resistance in front of IN+ & IN- pins of MAX49925 device?
3. Is there any formula or simulation is available to estimate the impact of MAX49925 device due to this configuration?