Post Go back to editing

Gain Error

Category: Datasheet/Specs
Product Number: MAX9920

Hi All

What is the error in gain and offset due to external resistors R at the input. Is there an equation which would allow it to be calculated. These resistors are part of a RC filter network.

Regards

ik

  • Hi 

    The MAX9920 typically has a Vsense of 200mV. It is necessary to confirm that the type Vsense is available at the input of MAX9920. Vos/Full Scale input would be the percentage of inaccuracy caused by the offset. Under the scenario that Vref=0V, the Gain Error across temperature specified in the datasheet would reach a maximum of 1.7%. Where your question was answered by me ?

    Regards

    PVP