Post Go back to editing

Neet to review the schematic

Category: Hardware
Product Number: AD8479

The customer asks for reviewing the schematic with AD8479.

They are developing BMS solution for UPS system with lead-acid battery.

It is designed as a discrete as the picture below. 

- Conditions

1. Common mode voltage of AD8479 is 600V.

2. the voltage of lead-acid battey is 14V.

3. 48 lead-acid battery are connected in series, and the total volatge is 672V.  

4. Trying to lower the voltage actually applied to AD8479 input terminal through voltage divide.

so that, they would like to know whether this was designed properly or not. 

please take a look at the schematic, and then please advice if there is any kind problem.

or if you have any other solution, please let me know it.