The MAX9611 is described in the Shutdown Current (ISHDN) section of the datasheet
** No activity on SCL **
Does this mean there is no activity on SCL after control register [SHDN=1]?
At this time, the power consumption of MAX9611 is about 5uA
Will the MAX9611 transition from shutdown mode to normal operating mode when SCL changes H/L?
(Or behind the address?)
Has the power consumption changed from 5uA=>1.6mA at this time?
Since there are many different devices on the I2C bus, we don't want the MAX9611 to switch from shutdown mode to normal operation when one of the devices receives an I2C signal, which would increase power consumption.