Post Go back to editing

Voltage measurement only

Category: Hardware
Product Number: LTC2945

Hi,

I am using the LTC2945 for voltage and power measurements, using the sense resistor. Now I want to measure the input voltage only, not using a sense resistor since there will be a high current. Is this possible? How to connect? There is no such example in the datasheet. But it is stated:

Sense+:

Supply Voltage and Current Sense Input. Used as
a supply and current sense input for the internal current
sense amplifier. The voltage at this pin is monitored by the
onboard ADC with a full-scale input range of 102.4V.

It is this ADC I want to use.

  • Hi  ,

    Good day. The onboard ADC can be access through the I2C capability of this part. The ADC continuously monitors three voltages in sequence: the differential voltage between Sense+ and Sense-, the Vdd or Vsense+ and VADIN. The sense pins can be biased independently of the part's supply voltage. Hence, you can monitor it using the onboard ADC.  Here is a the general data transfer for this part:

    To access the reading, you can set the CONTROL register's A5 and A6 to 10 respectively while enabling A2 pin for sense+ voltage monitoring. As shown in the table 3 of the datasheet:

    You can use the default configurations for the remaining bits. Based on this you can directly input the voltage on the sense+ pin. However, there should be no violation of the absolute max rating to avoid damaging the part. With this, I want to know your application's input voltage and current. I hope this helps.


    Regards,
    Gilbeys

  • Hi Gilbeys,

    Thanks for your answer. 

    To make sure I understand correct. If I connect the Sense- to reference/GND and then read the differential voltage between Sense+ and Sense- I should get the value I need. The input voltage will be between 10 and 40V, so should be well within specification.

    /Torbjörn

  • Hi  ,

    Good day. That should be the case. 


    Regards,
    Gilbeys