Post Go back to editing

AMP03 IVR specification and abs.max input voltage

Thread Summary

The user inquired about the meaning of IVR (Input Voltage Range) and the Input Voltage in the Absolute Maximum Ratings for the AMP03 difference amplifier. The final answer clarifies that IVR refers to the common mode voltage range, which can be up to ±20V, while the Input Voltage in the ABS Max table is the maximum voltage the input terminals can handle, typically ±15V for a dual supply. The AD8276 datasheet provides a similar discussion, and the internal voltage divider allows input voltages beyond the supply rails, up to 2 times the supply voltage, but the ±20V specification is guaranteed by CMR.
AI Generated Content
Category: Hardware
Product Number: AMP03

I'm a DFAE in Japan.

My customer sent me questions about AMP03 datasheet descriptions.

what does "IVR" mean in ELECTRICAL CHARACTERISTICS table,  |+IN - -IN| ?

what does "Input Voltage" of Absolute Maximum Ratings mean, terminal voltage? 

He likes to understand the descripancy between "IVR" and "Supply Voltage".

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.