Post Go back to editing

I have made a Schematic for MAX12900. Can someone verify it?

Thread Summary

The user seeks verification for a loop-powered 4-20 mA control circuit using the MAX12900, following the recommended schematic from the datasheet. The final answer indicates that only Maxim ATE products are currently supported on EngineerZone, directing the user to technical support pages for further assistance. The accompanying answer notes that Analog Devices will be on annual shutdown from December 24, 2022, to January 2, 2023, and suggests community assistance in the meantime.
AI Generated Content

Hello, I have made a schematic for MAX12900. I am using it to control a 4-20 mA loop. The circuit is loop powered. So I am using a DC-DC converter to power up the circuit. I have followed the recommended circuits from datasheet. Can someone please verify it?

Thanks in Advance.

PDF

Edit Notes

Added tag.
[edited by: emassa at 5:46 PM (GMT -5) on 5 Jan 2023]

Thread Notes

Parents Reply Children
No Data