Post Go back to editing

AD8479: maximum Vs in single supply operation

Dear sirs,

in AD8479 datasheet I could not find what is the maximum +Vs voltage that can be used in single supply operation (-Vs tied to ground).

It is only specified the maximum dual supply voltage (i.e. +-18V).

I would think that in single supply the maximum is 0/+36V but I would like a confirmation.

Thank you,

Riccardo

  • Hi Riccardo,

    What you are thinking is correct. For AD8479, the absolute maximum would be 0/V+36V during single supply operation.
    But please do take note that the datasheet only guarantees the electrical specifications at Vs= +/-15V. 
    Also, please do follow the guidelines about single supply operation stated in page 13 of the datasheet.

    That is all.

    Thank you and Best Regards,.
    Sham