Post Go back to editing

AD5749 counterpart current sense receiver Amplifier 4-20mA

Hi ADI Team,

I am looking for a current sense receiver amplifier application note, guideline, ref design for the AD5749 that is used in CN-0533 interfacing with ADXL1002

to interface with AD7768 as of CN-0540 ref design.

Any suitable amplifier part reference would be much appreciated, ideally around the ADA4945-1.

Thanks in advance.

Greetings,

Lala

Parents
  • Any feedback guys?

    As we moved forward with prototyping, we actually implemented a solution using AD8420 configured with a 50R load as 4-20mA current receiver and optionally also configured the ADA4945 as SE input stage with a 54R9 load resistor and calculated the FB path to amplify full scale minus some head-room. Waiting for the PCBA now to start testing.

Reply
  • Any feedback guys?

    As we moved forward with prototyping, we actually implemented a solution using AD8420 configured with a 50R load as 4-20mA current receiver and optionally also configured the ADA4945 as SE input stage with a 54R9 load resistor and calculated the FB path to amplify full scale minus some head-room. Waiting for the PCBA now to start testing.

Children