Post Go back to editing

About LT6106's Input

Thread Summary

The user inquires about the LT6106 current measurement in a bidirectional current path, specifically if connecting -IN to the load side causes issues. The final answer confirms that a reverse-current condition will not damage the part, and the output current will remain at zero. The user also asks about the maximum rating for +IN to V+ in reverse-current conditions, seeking confirmation if 0.5V or less is acceptable.
AI Generated Content


Hello,

I am considering LT6106 for current measurement.
In the case of a one-way current path, I think that it is used with "+IN is connected to the load side".

I am also thinking about the current flowing from the load side to VBATT.
In the case of a bidirectional current path, does setting "-IN is connected to the load side" cause a problem (deterioration or destruction)?

I understand that in a bidirectional current path, "+IN is connected to the load side" can measure the current value, and "-IN is connected to the load side" cannot measure the current value.

Best Regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.