Post Go back to editing

AD8488 applications questions

We are currently developing a wafer test solution and we are planning to use the AD8488 to benefit from his 128 channels to do high parallelism testing. We also plan to use the ADC AD9244 as advised in the AD8488 datasheet. The challenge for us is that we must measure very low current (in the 100pA range). We have some questions about the AD8488 functionality and performances.

  • How do we tune the integration time beyond 12µs? From my point of view, we must use the HOLD pin and let it at the high state for a longer time. Am I correct? And is there a maximum limit for the integration time?
  • If we want to slow down the output mux is it possible to slow down the clock (bellow 1MHz) during the output phase?
  • Do you have more explanation or information about the usage of the /WR pin? In the Figure 18 is mentioned a data line but I do not understand where I can access this data line and what am I supposed to send?
  • On page 3 of the datasheet I see that the CCR have a very large span +/- 26% which is quite huge. I was wondering if it is possible to do a calibration on one of the 128 channel and then applied it to all. I am basing this hypothesis on the fact that Figure 7 show a very stable value of CCR across the 128 channels.
  • Is the signal TFT_GATE an internal signal?
  • When the SWIRST and CF switch are open, what is the leakage current on the analog input?
  • Do you have an application schematic with the ADC?
  • Do you have a procedure to perform a current calibration of the channels

Regards

Parents Reply Children
No Data