Post Go back to editing

LT6118 as a fast-acting fuse with POR

I have implemented an LT6118 in a power supply and it is working pretty much as expected; when the current is over the specified limit, the pass transistor switches off. 12V input / 1.2A trip current. I attach a schematic (which looks blurry). I hope it is readable.

My issue is with the suggested method of LE transparency on start-up. I have used the circuit in the datasheet to delay the LE function using an RC delay (24k9 + 100n). This does not prevent the latch working when switched on.

Measuring the LE voltage shows that the voltage doesn't drop below 0.5V for a long time - far longer than the time between switch-ons. Therefore, the latch is always enabled.

Although the datasheet suggests a circuit for POR, this doesn't seem to function as expected. Even when starting from around 0V, the rise-time is extremely short.  I have increased the value of R in the RC circuit but the rise time is still in the order of uS, not 100uS. The input is a switched 12V supply which is always present, so there is no rise-time - it is a step.

What is the expected behaviour of the POR? Nothing I've seen so far makes me think the POR actually works as per the data sheet.

Thanks in advance.

  • Hi village,

    Thank you for using the LT6118 on your application.

    Checking the Power-on reset feature of the LT6118, it states that the voltage level of LE pin needs to remain below VIL threshold of 0.5V for at least 100 us. And the circuit to achieve this behavior is entirely based on the RC charging behavior (there are a lot of articles online regarding this if you want a detailed explanation), and given the RC value you used (24.9k and 100nF), Vs (12V) and the formula:

    The voltage level across capacitor (Vcap) should be around 0.47V at 100us, according to the datasheet this should be enough to have the correct state of the comparator output on startup. Given that you're not seeing this charging on your end, may I know what instrument you are using in measuring the charging curve (type of probe) (since we're dealing with small value capacitor this may affect the capacitance when trying to measure) and the type of resistor and capacitor you are using? I hope this helps village.

    Best Regards,
    Dann