Post Go back to editing

ADN2880 for phase measurement

Thread Summary

The user inquired about phase shift in ADN2880's output voltage when approaching or exceeding the 260mVp-p differential swing, and requested estimated input current, bandwidth, and transimpedance for a 1.5pF input capacitance. The ADN2880 is not characterized as a linear amplifier, but with a 1.5pF photo-diode, the expected 3dB bandwidth is around 833MHz. Input current range and transimpedance gain are provided in the datasheet.
AI Generated Content


My application is precise optical phase measurement.

I am curious if there would be a phase shift as the output voltage from ADN2880 approaches to or goes over the maximum differential swing which is 260mVp-p.

Can you also provide me the estimated values for input current, bandwidth, and transimpedance when the input capacitance is 1.5pF?

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.