Post Go back to editing

Problem in AD8219 Spice macro model

Hello,

I have included the spice macro model of AD8219 given here into my LTSpice system trying to sense the current passing through a precision sense resistor of 1mOhm where the current I am sensing has the range of 0A up to 10A. In my application, the AD8219 will be powered from 5V standalone supply while the common-mode voltage would be typically at 36V. Below I am including a schematic for testing the spice mode. The problem is that no matter what is the value of current passing thourgh my sense resistor, the output of AD8219 is always fixed at 5.6V

Is it an issue in the spice model or something in my simulation schematic?

Thanks
 



corrected link to AD8219 page
[edited by: msaad@earthdas.com at 12:07 PM (GMT 0) on 10 Jun 2020]