See attachment.
AD8210
Production
The AD8210 is a single-supply, difference amplifier ideal for amplifying small differential voltages in the presence of large common-mode voltages. The...
AD8210 on Analog.com
AD8211
Production
The AD8211 is a high voltage, precision current shunt amplifier. It features a set gain of 20 V/V, with a typical ±0.35% gain error over the entire temperature...
AD8211 on Analog.com
AD8213
Production
The AD8213 is a dual-channel, precision current sense amplifier. It features a set gain of 20 V/V, with a maximum ±0.5% gain error over the entire temperature...
Datasheet
AD8213 on Analog.com
AD8215
Production
The AD8215 is a high voltage, precision current shunt monitor. It features a set gain of 20 V/V, with a maximum ±0.3% gain error over the entire temperature...
Datasheet
AD8215 on Analog.com
See attachment.
This important information is very well hidden! A hint in the data sheet (section Applications Information, paragraph HIGH-SIDE CURRENT SENSE WITH A HIGH-SIDE SWITCH) would have saved us from quite some time searching for the mistake in our circuit.
Glad to have found the explanation now, anyway. Thanks.
This important information is very well hidden! A hint in the data sheet (section Applications Information, paragraph HIGH-SIDE CURRENT SENSE WITH A HIGH-SIDE SWITCH) would have saved us from quite some time searching for the mistake in our circuit.
Glad to have found the explanation now, anyway. Thanks.