Post Go back to editing

AD8276

Hi,

I have some problems with a AD8276 after some hours the circuit burns off.

the power supply is +/- 13 volts. The input signal does not exceed 10 volts and the load of the circuit in a 20kohms  resistor.

do you have a explanation

best regard

George,

  Does the circuit work normally for several hours and then stop?

When you say "burns off", do you mean the part fails completely? (burns up?)

Do you have +/-10V on the inputs with no power supplies?

Under normal operation, does the part get hot?

Is this more than one pc board?

Harry


  • Harry,

    Yes the circuit works normally for several hours The part doesn't burn up in normal operation for the moment

    The part fails completely and there is a little hole (see picture) but I must say that

    the part burn up after that I switch off the power supplies and then switch on in fact I design a board. On this board there is a micro controller so I restart from time to time the power supplies.

    Yes some time i Have 5 Volts ( signal generator) on the inputs with no power supplies

    The part is not hot when it burns up and I think that  it  burns up  quickly

    Georges

  • Hi Georges,

    Are you able to share any information about your application, or possibly schematic? Typically, when I've seen this kind of failure it is due to very high transients being applied to the inputs, which exceed the 42V tolerance of the device. If the supply has excessive overshoot, that can also break down the part, eventually leading to catastrophic failure.

    Any such information would be helpful!

    Cheers,

    -David

  • Hi David

    The inputs is connected to a tektronix AFG3000 signal generator via a twist paire. it's outputs cannot exceed 10 Volts. The output part is connected to operational amplifier ( inverting ) via a 20K ohms resitor. The only explanation that I see is when I switch off switch on the rack power supplies there are some transients. however I placed two capacitors near the +/- pin power supplies. The power supplies is a linear power supply, I connected all the ground of the rack  in the same point (Electromagnetic compatibility rules). I cannot give you a schematic for the moment because I am at home and I am in vacation for 3 weeks. I 'll send you the schematic and a picture of the rack when I 'll come back to work.

    Cheer

    Georges

  • Geroge,

      It might also be power supply sequencing.  On some parts, it makes a difference whether the

    plus supply or the minus supply comes up first.  You could try it both ways and see if one is

    worse than the other.

    Harry


  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin