Post Go back to editing

AD8479 as a shunt voltage amplifier in a large DC Motor

Thread Summary

The user needs to monitor 0-120mV shunt voltage representing 0-1200A in a 0-550VDC motor, connecting to a 3.3V ADC input on an STM32 microprocessor. The AD8479 is not suitable due to its output not swinging to 0V and potential risk to the microprocessor's analog input. The engineer suggests using a series resistor and diode for protection or an alternative amplifier like the ADA4177 to gain up the signal. The user is considering other options and is looking for a product that can handle high common mode voltages.
AI Generated Content

We need to monitor the voltage across a shunt in a large DC motor, the Motor voltage is 0 ~ 550VDC and the shunt voltage = 0 ~ 120mV to represent the 0 ~ 1200 Amps flowing into the armature, the signal from the shunt amplifier output will connect to a 3.3VDC analog input on a microprocessor (STM32 Arm Cortex Micro) where the logic is used to control the motor. The concern is that we need to be sure that the output from (for instance) a AD8479 will not damage the analog input on the Microprocessor. The resistance of the shunt is very low due to the current flowing through being very high. Should we be using an AD8217 instead?

We have VCC supply at 3.3VDC or 5VDC or 24VDC.

Are we suggesting the correct AD chip for this application? Is there a standard circuit for what we are trying to achieve?

Finally, we could alternatively use a chip with a serial SPI bus if there is such a chip available for measuring shunt voltages without the risk of the ground in the micro being affected by the 550VDC motor supply. The voltage when measured between the shunt and ground is floating, they are not connected in any way.

Any advice or assistance would be very much appreciated.

Cheers

Rudy.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.