AD5560
Production
The AD5560 is a high performance, highly integrated device power supply consisting of programmable force voltages and measure ranges. This part includes...
Datasheet
AD5560 on Analog.com
Hello,
I have some quetions about current clamps AD5560.
1) If i do not use offset (CLH, CLL), it is mean that current range is simmetrical (for example -500 mA to 500 mA)
2) I use current range -25...25 mA, then i set CLH 18,75 mA - measuring value is ~ 21 mA, CLL -18,75 mA -measuring value is ~ -20,6 mA. For other points i have the same offset current (for every current range). Is it correct? How can I set current clamp more accuracy? By using register CLL DAC c, CLL DAC m, CLH DAC c, CLH DAC m?
3) What is the minimum current limit value? + 10% of full-scale current (according with datasheet DUT current can never exceed the programmed clamp limit + 10% of full-scale current)?
Thank you.
stephenv - Moved from Other Products (EN) to Specialty Amplifiers. Post date updated from Tuesday, February 11, 2020 10:46 AM UTC to Tuesday, February 3, 2026 9:03 PM UTC to reflect the move.
stephenv - Moved from Other Products (EN) to Specialty Amplifiers. Post date updated from Tuesday, February 3, 2026 9:03 PM UTC to Tuesday, February 3, 2026 9:03 PM UTC to reflect the move.
stephenv - Moved from Other Products (EN) to Specialty Amplifiers. Post date updated from Tuesday, February 3, 2026 9:03 PM UTC to Tuesday, February 3, 2026 9:04 PM UTC to reflect the move.
stephenv - Moved from Other Products (EN) to Specialty Amplifiers. Post date updated from Tuesday, February 3, 2026 9:04 PM UTC to Tuesday, February 3, 2026 9:04 PM UTC to reflect the move.