is there any info on the input resistance of the RS+ & RS-? (RG1 & RG2)
or any notes of how to filter any noise into RS+ & RS-?
I am trying to add and "RC" filter to reduce the noise into the ADM4073H
When I add the RC = 1k & 0.1uf, the ADM4073H gives the wrong output current
1k resistor from Rsense to RS+ and 1k resistor to RS-
0.1uf cap between RS+ & RS-
I am measuring the output current with a amp meter and the readings from the ADM4073 do not match,
they are as follows: amp meter = 4A, ADM4073 = 500mA (with the 1k resistor)
if I bypass the 1k resistors the readings are very similar.
What I need is an example of a filter circuit that can be added to the Rsense circuit (between RS= & RS-) to reduce the input noise
any comments will be appreciated
Thank you
Fausto bartra