Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Operational Amplifiers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Operational Amplifiers
  • Amplifiers
Operational Amplifiers
Documents Why is it, that voltage feedback amplifiers seem to dominant the op amp landscape compared to current feedback amplifiers?
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
Table of Contents
  • OPERATIONAL AMPLIFIERS
  • +ADA4177: FAQ
  • +ADA4528: FAQ
  • +ADA4622: FAQ
  • +ADA4638: FAQ
  • +AD8000: FAQ
  • +AD8005: FAQ
  • AD8005: FAQ
  • +AD8033: FAQ
  • +AD80419BBCZ: FAQ
  • +AD822: FAQ
  • +AD8397: FAQ
  • +AD8608: FAQ
  • +AD8622: FAQ
  • +ADA4077-2: FAQ
  • +ADA4098-1: FAQ
  • +ADA4350: FAQ
  • +ADA4500-2: FAQ
  • +ADA4622-1: FAQ
  • +ADA4661-2: FAQ
  • +ADA4661-2: FAQ
  • +ADUM3190: FAQ
  • +LTC6078: FAQ
  • +MAX4238: FAQ
  • +OP1177: FAQ
  • +OP2177: FAQ
  • +OP27: FAQ
  • +OP297: FAQ
  • +OP37: FAQ
  • +OP484S: FAQ
  • +precision performance of an amplifier: FAQ
  • -voltage feedback amplifiers: FAQ
    • Why is it, that voltage feedback amplifiers seem to dominant the op amp landscape compared to current feedback amplifiers?

Why is it, that voltage feedback amplifiers seem to dominant the op amp landscape compared to current feedback amplifiers?

Why is it, that voltage feedback amplifiers seem to dominant the op amp landscape compared to current feedback amplifiers?

Some may argue when it comes to selecting an op amp, it's more of a personal preference or taste in amplifiers. That is probably why quite often engineers select voltage feedback (VFB) op amps over current feedback (CFB) op amps.

So why is that? Well I'm sure that there are lots of reasons, just the sheer numbers, there are a lot more VFB amplifiers than CFB to chose from, but another reason is education. In colleges most often voltage feedback is the standard that is taught in the classroom. Many of the op amp examples found in text books, labs or simulations focus on VFB. You'll find very few examples of CFB op amps described in college text books, and if you do, they will only be briefly mentioned.

Now we can’t possibly cover all the differences and options between current feedback and voltage feedback amplifiers here, but we can discuss a few key points. First the design equations used for voltage feedback amps work equally well for current feedback amps, so nothing new to learn there. Voltage feedback amplifiers have a fixed gain bandwidth product; current feedback amplifiers do not, so you can have high gain and high bandwidth with a CFB amp. Voltage feedback amps have two high input impedance nodes, current feedback amps only have one, the non-inverting input; the inverting input is a low impedance input. Voltage feedback amplifiers have "open loop gain"; current feedback amps have "open loop transimpedance". Current feedback amplifiers have very wide bandwidths and very high slew rates compared to VFB amps. The feedback resistor plays a large role in CFB amplifier stability, unlike voltage feedback amplifiers. This limits the choices of feedback resistor (the value can be found in the manufacturer's datasheet) it can also limit the value of the gain set resistor.

We've only scratched the surface here, regarding current and voltage feedback amplifiers. Current feedback amplifiers provide engineers with another powerful option when designing circuits. We have a great deal of additional information on current feedback and voltage feedback amplifiers which can be accessed by clicking on the links below.

http://www.analog.com/static/imported-files/tutorials/MT-034.pdf

http://www.analog.com/static/imported-files/tutorials/MT-058.pdf

http://www.analog.com/static/imported-files/tutorials/MT-060.pdf

http://www.analog.com/library/analogDialogue/Anniversary/22.html

http://www.analog.com/library/analogDialogue/Anniversary/23.html

  • Share
  • History
  • More