Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
Operational Amplifiers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Operational Amplifiers
  • Amplifiers
Operational Amplifiers
Documents ADA4177: How much above and below the supply voltages can I drive the input?
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
Table of Contents
  • OPERATIONAL AMPLIFIERS
  • -ADA4177: FAQ
    • What power-supply considerations affect the precision of the ADA4177?
    • ADA4177: Besides over-voltage protection, are there any other robustness features?
    • ADA4177: How much above and below the supply voltages can I drive the input?
    • ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?
    • ADA4177: What is the advantage of using integrated over-voltage protection instead of building it external to an op amp’s inputs?
    • ADA4177: What resistor values should I use around the amplifier?
    • ADA4177: Why do I need a rail-to-rail output (RRO)?
    • Will the ADA4177 drive an Analog-to-Digital Converter?
  • +ADA4528: FAQ
  • +ADA4622: FAQ
  • +ADA4638: FAQ
  • +AD8000: FAQ
  • +AD8005: FAQ
  • AD8005: FAQ
  • +AD8033: FAQ
  • +AD80419BBCZ: FAQ
  • +AD822: FAQ
  • +AD8397: FAQ
  • +AD8608: FAQ
  • +AD8622: FAQ
  • +ADA4077-2: FAQ
  • +ADA4098-1: FAQ
  • +ADA4350: FAQ
  • +ADA4500-2: FAQ
  • +ADA4622-1: FAQ
  • +ADA4661-2: FAQ
  • +ADA4661-2: FAQ
  • +ADUM3190: FAQ
  • +LTC6078: FAQ
  • +MAX4238: FAQ
  • +OP1177: FAQ
  • +OP27: FAQ
  • +OP297: FAQ
  • +OP37: FAQ
  • +OP484S: FAQ
  • +precision performance of an amplifier: FAQ
  • +voltage feedback amplifiers: FAQ

ADA4177: How much above and below the supply voltages can I drive the input?

The integrated over-voltage protection (OVP) of the ADA4177 allows the inputs of the amplifier to be driven to a voltage up to 32 V above the positive supply voltage or 32 V below the negative supply voltage without damage to the device.  The ADA4177 has an operating voltage limit of 30V so, for example, when biased at ±15V, the input can safely range from +47V to -47V.