Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Operational Amplifiers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Operational Amplifiers
  • Amplifiers
Operational Amplifiers
Documents ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel

Products Mentioned

ADA4177-1 Recommended for New Designs
The ADA4177-1 single-channel, ADA4177-2 dual-channel, and ADA4177-4 quad-channel amplifiers feature low offset voltage (2 μV typical) and drift (1 μV...
Datasheet
ADA4177-1 on Analog.com

ADA4177-2 Recommended for New Designs
The ADA4177-1 single-channel, ADA4177-2 dual-channel, and ADA4177-4 quad-channel amplifiers feature low offset voltage (2 μV typical) and drift (1 μV...
Datasheet
ADA4177-2 on Analog.com

ADA4177-4 Recommended for New Designs
The ADA4177-1 single-channel, ADA4177-2 dual-channel, and ADA4177-4 quad-channel amplifiers feature low offset voltage (2 μV typical) and drift (1 μV...
Datasheet
ADA4177-4 on Analog.com

Table of Contents
  • OPERATIONAL AMPLIFIERS
  • -ADA4177: FAQ
    • What power-supply considerations affect the precision of the ADA4177?
    • ADA4177: Besides over-voltage protection, are there any other robustness features?
    • ADA4177: How much above and below the supply voltages can I drive the input?
    • ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?
    • ADA4177: What is the advantage of using integrated over-voltage protection instead of building it external to an op amp’s inputs?
    • ADA4177: What resistor values should I use around the amplifier?
    • ADA4177: Why do I need a rail-to-rail output (RRO)?
    • Will the ADA4177 drive an Analog-to-Digital Converter?
  • +ADA4528: FAQ
  • +ADA4622: FAQ
  • +ADA4638: FAQ
  • +AD8000: FAQ
  • +AD8005: FAQ
  • AD8005: FAQ
  • +AD8033: FAQ
  • +AD80419BBCZ: FAQ
  • +AD822: FAQ
  • +AD8397: FAQ
  • +AD8608: FAQ
  • +AD8622: FAQ
  • +ADA4077-2: FAQ
  • +ADA4098-1: FAQ
  • +ADA4350: FAQ
  • +ADA4500-2: FAQ
  • +ADA4622-1: FAQ
  • +ADA4661-2: FAQ
  • +ADA4661-2: FAQ
  • +ADUM3190: FAQ
  • +LTC6078: FAQ
  • +MAX4238: FAQ
  • +OP1177: FAQ
  • +OP2177: FAQ
  • +OP27: FAQ
  • +OP297: FAQ
  • +OP37: FAQ
  • +OP484S: FAQ
  • +precision performance of an amplifier: FAQ
  • +voltage feedback amplifiers: FAQ

ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?

Yes. When either input exceeds the rail by more than a diode, large currents flow through the protection JFETs which causes the channels to pinch off and effectively raises their resistance. The ADA4177 will dissipate heat according to the thermal resistance (θJA) of the package it is in, which, in turn, heats up the die. The die temperature must not the absolute maximum rating of 150°C for device protection. Extended over-temperature exposure can cause some operating specifications to shift outside of their guaranteed limits.

Tags: over_voltage ada4177
  • Share
  • History
  • More