Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
Operational Amplifiers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Operational Amplifiers
  • Amplifiers
Operational Amplifiers
Documents ADA4177: Why do I need a rail-to-rail output (RRO)?
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
Table of Contents
  • OPERATIONAL AMPLIFIERS
  • -ADA4177: FAQ
    • What power-supply considerations affect the precision of the ADA4177?
    • ADA4177: Besides over-voltage protection, are there any other robustness features?
    • ADA4177: How much above and below the supply voltages can I drive the input?
    • ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?
    • ADA4177: What is the advantage of using integrated over-voltage protection instead of building it external to an op amp’s inputs?
    • ADA4177: What resistor values should I use around the amplifier?
    • ADA4177: Why do I need a rail-to-rail output (RRO)?
    • Will the ADA4177 drive an Analog-to-Digital Converter?
  • +ADA4528: FAQ
  • +ADA4622: FAQ
  • +ADA4638: FAQ
  • +AD8000: FAQ
  • +AD8005: FAQ
  • AD8005: FAQ
  • +AD8033: FAQ
  • +AD80419BBCZ: FAQ
  • +AD822: FAQ
  • +AD8397: FAQ
  • +AD8608: FAQ
  • +AD8622: FAQ
  • +ADA4077-2: FAQ
  • +ADA4098-1: FAQ
  • +ADA4350: FAQ
  • +ADA4500-2: FAQ
  • +ADA4622-1: FAQ
  • +ADA4661-2: FAQ
  • +ADA4661-2: FAQ
  • +ADUM3190: FAQ
  • +LTC6078: FAQ
  • +MAX4238: FAQ
  • +OP1177: FAQ
  • +OP27: FAQ
  • +OP297: FAQ
  • +OP37: FAQ
  • +OP484S: FAQ
  • +precision performance of an amplifier: FAQ
  • +voltage feedback amplifiers: FAQ

ADA4177: Why do I need a rail-to-rail output (RRO)?

There are many situations in which an RRO optimizes the system design. For example, since the ADA4177 has a rail-to-rail output, it can be powered from an ADC’s reference, allowing the op amp’s output signal to swing almost the full range of the reference. This allows the system designer to achieve more gain with one amplifier and maximize the ADC’s input signal dynamic range.