• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Operational Amplifiers
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Operational Amplifiers
  • Amplifiers
Operational Amplifiers
Documents ADA4177: What resistor values should I use around the amplifier?
  • Q&A
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
Table of Contents
  • OPERATIONAL AMPLIFIERS
  • -ADA4177: FAQ
    • What power-supply considerations affect the precision of the ADA4177?
    • ADA4177: Besides over-voltage protection, are there any other robustness features?
    • ADA4177: How much above and below the supply voltages can I drive the input?
    • ADA4177: If the inputs range beyond the supply voltages, do I need to concern myself with the load current (that is, the total power of the device)?
    • ADA4177: What is the advantage of using integrated over-voltage protection instead of building it external to an op amp’s inputs?
    • ADA4177: What resistor values should I use around the amplifier?
    • ADA4177: Why do I need a rail-to-rail output (RRO)?
    • Will the ADA4177 drive an Analog-to-Digital Converter?
  • +ADA4528: FAQ
  • +ADA4622: FAQ
  • +ADA4638: FAQ
  • +AD8000: FAQ
  • +AD8005: FAQ
  • AD8005: FAQ
  • +AD8033: FAQ
  • +AD80419BBCZ: FAQ
  • +AD822: FAQ
  • +AD8397: FAQ
  • +AD8608: FAQ
  • +AD8622: FAQ
  • +ADA4077-2: FAQ
  • +ADA4098-1: FAQ
  • +ADA4350: FAQ
  • +ADA4500-2: FAQ
  • +ADA4622-1: FAQ
  • +ADA4661-2: FAQ
  • +ADA4661-2: FAQ
  • +ADUM3190: FAQ
  • +LTC6078: FAQ
  • +MAX4238: FAQ
  • +OP1177: FAQ
  • +OP27: FAQ
  • +OP297: FAQ
  • +OP37: FAQ
  • +OP484S: FAQ
  • +precision performance of an amplifier: FAQ
  • +voltage feedback amplifiers: FAQ

ADA4177: What resistor values should I use around the amplifier?

ADA4177 has a low voltage noise density of 8 nV/√Hz, only twice the Johnson noise of a 1kΩ resistor.  Placing a 1KΩ resistor with thermal noise of 4 nV/√Hz at the input of the amplifier increases total input referred noise to 8.9 nV/√Hz.  It is important to use low value resistors around a low-noise amplifier.