KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT1886
Production
The LT1886 is a 200mA minimum output current dual op amp with outstanding distortion performance. The amplifiers are gain-of-ten stable, but can be easily...
Datasheet
LT1886 on Analog.com
Hi,
I am trying to design a 4th order Butterworth low pass filter with the following parameters:
- cut off frequency at 20MHz to filter some noise on an input signal.
- I do not want any gain
- V+ = 3.3V and V- = GND
After calculation and simulation i came up with the following design using a pair of LT1886 OpAmp.
But when i connect this onto my design, it generates a lots of ringing on the input "IN1" and OpAmp output making the input and output signals even worse. When i disconnect the circuit, the input is pretty clean, so something is making my design goes wrongly.
Any input on how to improve the current design would be appreciated.
Thanks
Here are a few things to consider regarding this filter design:
1) LT1886 is NOT unity gain stable. What that means is that it must always operate with closed-loop gain Av >= 10V/V, or it will be unstable and oscillate. It can be used for gains < 10, but it requires an external compensation capacitor in order to make sure it stays stable, as described on p. 10 of the datasheet.
The way the output is tied to -IN for both LT1886's in this design guarantees unity gain, which means this op-amp is guaranteed NOT to be stable. Simulations may not show this correctly since this kind of behavior is hard to capture in models, so I would recommend NOT relying exclusively on simulations to know whether something will ring or not. Bench results are the only way to be sure.
2) Stacking multiples of the same poles causes the -3dB point to shift. Since the two sections of this filter are identical, there are two of each pole. When poles are stacked, their effects are doubled, so two poles in the same location lead to a -6dB point, not a -3dB point, at the frequency of choice. This means the cutoff will be below the desired 20MHz.
3) The Sallen-Key architecture as shown is vulnerable to capacitive drive problems. The output of the first amplifier is connected directly via feedback to C6, 220pF. At 20MHz, the impedance presented by C6 is only 36 Ohm, so the op-amp's output also sees C5, 120pF via the 47 Ohm R6, since 47 Ohm is not large enough to isolate the second capacitor. Although bigger resistors add noise, a resistor at least comparable to the impedance presented by the caps is necessary to isolate the caps from the output of the op-amp.
Most op-amps will oscillate or ring if they are driving significant capacitance. For LT1886 in particular, on p 6, the plot "Frequency Response vs Capacitive Load" shows 6dB of gain peaking at 60-70MHz while driving 200pF alone, and the peaking only gets larger and lower in frequency as more cap load is added. A significant gain peak leads to ringing too, since a gain above 1 will be present at a frequency when the poles' effect has started knocking the phase margin down.
Given all of these significant problems, I would recommend a different design approach. Here are two designs that should meet your requirements, for a 3rd and a 7th order Butterworth-equivalent filter at 20MHz cutoff that is free of all of the above problems.
Please let me know if you have further questions.
Here are a few things to consider regarding this filter design:
1) LT1886 is NOT unity gain stable. What that means is that it must always operate with closed-loop gain Av >= 10V/V, or it will be unstable and oscillate. It can be used for gains < 10, but it requires an external compensation capacitor in order to make sure it stays stable, as described on p. 10 of the datasheet.
The way the output is tied to -IN for both LT1886's in this design guarantees unity gain, which means this op-amp is guaranteed NOT to be stable. Simulations may not show this correctly since this kind of behavior is hard to capture in models, so I would recommend NOT relying exclusively on simulations to know whether something will ring or not. Bench results are the only way to be sure.
2) Stacking multiples of the same poles causes the -3dB point to shift. Since the two sections of this filter are identical, there are two of each pole. When poles are stacked, their effects are doubled, so two poles in the same location lead to a -6dB point, not a -3dB point, at the frequency of choice. This means the cutoff will be below the desired 20MHz.
3) The Sallen-Key architecture as shown is vulnerable to capacitive drive problems. The output of the first amplifier is connected directly via feedback to C6, 220pF. At 20MHz, the impedance presented by C6 is only 36 Ohm, so the op-amp's output also sees C5, 120pF via the 47 Ohm R6, since 47 Ohm is not large enough to isolate the second capacitor. Although bigger resistors add noise, a resistor at least comparable to the impedance presented by the caps is necessary to isolate the caps from the output of the op-amp.
Most op-amps will oscillate or ring if they are driving significant capacitance. For LT1886 in particular, on p 6, the plot "Frequency Response vs Capacitive Load" shows 6dB of gain peaking at 60-70MHz while driving 200pF alone, and the peaking only gets larger and lower in frequency as more cap load is added. A significant gain peak leads to ringing too, since a gain above 1 will be present at a frequency when the poles' effect has started knocking the phase margin down.
Given all of these significant problems, I would recommend a different design approach. Here are two designs that should meet your requirements, for a 3rd and a 7th order Butterworth-equivalent filter at 20MHz cutoff that is free of all of the above problems.
Please let me know if you have further questions.