Hello everyone
I want to simulate my circuit with LTspice, but can not find the model of ADA4062-4, does anyone know a similar spice mode to ADA4062-4?
best ragards.
YQ
ADA4062-4
Production
The ADA4062-2 and ADA4062-4 are dual and quad JFET-input amplifiers with industry-leading performance. They offer lower power, offset voltage, drift, and...
Datasheet
ADA4062-4 on Analog.com
Hello everyone
I want to simulate my circuit with LTspice, but can not find the model of ADA4062-4, does anyone know a similar spice mode to ADA4062-4?
best ragards.
YQ
Hi Goz
thanks to your quick reply!!
The application is about body probe electronics.
Best Regards.
YQ
Hi Goz
I made a simulation of Figure 59. Notch Filter Circuit and got the result as following.
As it shows, the circuit has a good spec. at 60Hz, but the gain from nearly 11MHz rise up, and have a peak about 5dB at 61MHz.
There are not much information about above 100MHz in datesheet.
Could you tell me if the result is right? or whether the mode fit the high frequency simulation.
Besr Regards.
YQ
Hi,
As seen on the Open-loop gain and Phase vs Frequency plot on the ADA4062 datasheet, at gain of 1, the correct response should be deteriorating or decaying. This might be a bug on the SPICE model and we'll try to fix it.
Should you have any concerns let us know.
Best Regards,
Goz
Hi Goz
thanks a lot for your confirmation. and sorry for the late reply.
please let me know if you do the fix.
Best Regards
YQ