Hello,
I have a question about LT1362 from our customer.
In the absolute maximum ratings, the Differential Input Voltage is explained as followings.
Differential Input Voltage
(Transient Only) (Note 2).......... ±10V
and the "Note2" is as followings.
Note 2: Differential inputs of ±10V are appropriate for transient operation
only, such as during slewing. Large, sustained differential inputs will cause
excessive power dissipation and may damage the part.
The customer wants to know the maximum rating of constant voltage which are input to differentional input, not a transient.
Could you please tell the maximum differential input level of DC to me ?
Best regards,
ysuzuki