Post Go back to editing

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN  and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application a

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as when Input voltage is higher than the supply voltage.  If not can i have a drop in replacement of that IC which are having such capability as i cant change the design now. opamp

Parents Reply Children
No Data