Post Go back to editing

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as whe

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as when Input voltage is higher than the supply voltage.  If not Can i have a drop in replacement for this IC with the IC's which are having such capability as i cant change the design now. high-current opamp opamp