SPICE Model for AD8610 does not work

I'm using the AD8610 in a simple buffer application. AD8627 and ADA4622 are working as expected but in the prototype i am bound to the AD8610. See the part of the simulation below.

Followup: I tried also to eliminate R1, R2, C1 and C2, same result

AGND is just a virtual GND for the single supplied circuit and should have a voltage of 2.5V. The right side is a square voltage generator with the AGND as offset. The pp-voltage is 400mV and the AD8610 acts as buffer. Here is what the waves should look like (simulated with AD8627):

v(generator) and v(generator_out) are congruent... v(agnd) is 2.5V

Now the waves with original AD8610 spice model:

v(generator_out) is wrong.

I compared both models and found a way to make the circuit run, but I have no idea what the changed parameter does actually or where I can find it in the datasheet. Hope anyone can help me.

Left: AD8627 / right: AD8610

If I change V3 to 5 or something the circuit works correct. What is V2 and V3 for? Are the values correct?

Thanks in advance and best regards

Fabian

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:05 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:05 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data