Post Go back to editing

No output observed on the Vref1 and Vout1 pin of ADUM3195 , but there is output on Vout2

Thread Summary

The user is troubleshooting an ADUM3195 buffer where VOUT1 (pin 6) shows no output and VREF1 (pin 4) is not generating 2.5V. The final answer suggests checking VDD1 (pin 1) for a voltage between 4.5V and 5.5V, ensuring no capacitor is on VREF1, and confirming that pin 7 is tied to GND1. If these checks are correct, the user is advised to share the schematic and measured VDD1.
AI Generated Content
Category: Hardware
Product Number: ADUM3195

Hi,

We were using ADUM3195 as buffer , we are feeding 2.5V into the non inverting terminal (pin 12) .  We observed 2.5V on Vout2 (pin 10) as expected . 

Issue : When we were observing Vout1 (pin 6) , there were no output . Additionally we saw that the internal reference generator on the Vout1 side (pin 4) not generating 2.5V as well so I am assuming the demodulator is not getting powered.

Could you help us troubleshoot this ?

This is very urgent as we are in a critical testing phase of our design , prompt help will be greatly appreciated.

Regards,

Anway 

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.