Post Go back to editing

TIA configuration

Thread Summary

The user inquires about reconfiguring the ADA4530-1R-EBZ-TIA Evaluation Board for BUF operation. The final answer confirms that the board can be reconfigured by replacing RF1 with 0 Ω, populating JP1 with 0 Ω, and removing JP2 and RS1 resistors. The existing BNC connector can be used for basic buffer operation, but a triaxial connector is needed for guarded input measurements. Cleaning the board after rework is essential to maintain low leakage performance.
AI Generated Content
Category: Hardware
Product Number: ADA4530-1

Hello,

I have the ADA4530-1 Evaluation Board, part number ADA4530-1R-EBZ-TIA.

According to the datasheet, the board appears to support reconfiguration between the basic, TIA, and BUF configurations. I need to use it in the BUF configuration.

Can the existing board be reconfigured for BUF operation by changing the resistor configuration, or are there any hardware differences between the TIA and BUF versions that would prevent this?

Thank you for your help.

  • Hi  

    Yes, the ADA4530-1R-EBZ-TIA can be reconfigured for unity-gain buffer operation.

    Based on Figures 24 and 25 of the UG-865 User Guide, the required component changes are:

    • RF1: Replace the 10 GΩ resistor with 0 Ω.
    • JP1: Populate with 0 Ω.
    • JP2: Remove the 0 Ω resistor.
    • RS1: Remove the 0 Ω resistor.

    The main hardware difference is the input connector. The TIA board uses a BNC connector, while the BUF board uses a triaxial connector that provides a separate guard connection.

    The existing BNC connector can be retained for basic buffer operation. However, if the application requires a guarded input for very low leakage measurements, the input connection must also be modified accordingly.

    Please also ensure that the board is properly cleaned after rework, as described in UG-865, to maintain its low leakage performance.

    Best Regards,
    Ian

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.