Post Go back to editing

AD8655 SPICE model: Is input current noise included?

Category: Datasheet/Specs

Hello,

I'm planning to simulate the AD8655. Does the AD8655 SPICE model include input current noise?

If it does, could you tell me how to confirm this, for example from the model netlist or the LTspice noise analysis results?

This is for a high-impedance circuit (10–20 MΩ), so input current noise is a major concern for us.

Thank you in advance.

  • Hi  

    The AD8655 SPICE model includes input voltage noise, with 1/f, but not input current noise.

    To confirm this in LTspice, you can run a .noise analysis and look at the per-device noise contributions in Add Traces. The op amp's internal noise source has En, In and Icm terms. In my test, a follower with a noiseless 1 Ω–1 GΩ source resistor, In and Icm were zero at every frequency. All of the op amp's noise came from En.

    AD8655 datasheet does not include a current noise specification, but as a rough estimate, the shot noise from IB (1 pA typ) is about √(2q·IB) ≈ 0.6 fA/√Hz. On 20 MΩ that's about 11 nV/√Hz, well below the resistor's own thermal noise of about 575 nV/√Hz. If you need to, you can add a noise current source at the input. For the meantime, I will bring this up to the LTspice team.

    Best Regards,
    Ian

  • Hi,

    Thank you for the clarification.

    I understand that the current AD8655 SPICE model does not include input current noise.

    Could you please show me how to add an equivalent noise current source at the input and simulate in LTspice?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.