Post Go back to editing

AD8465 SDNn pin information

Thread Summary

The user inquired about the SDNn pin of the AD8465: 1) It should be driven to a valid logic level (VIL ≤ 0.6V for shutdown, VIH ≥ 2.0V for normal operation) and not left floating. 2) SDN is referenced to VCCO, with its high-level specification extending up to VCCO and input-high current specified at VIH = VCCO.

View FAQ
AI Generated Content
Category: Hardware
Product Number: AD8465

The AD8465 datasheet does not seem to say much about the SDNn pin. I would like to know two things:

1. Is it internally pulled up? Or does it always need a valid level?

2. Is it referred to VCCO?
The Absolute Maximum Ratings show SDNn as having a max voltage of "VCCO + 0.5 V ", but the diagram on first page shows it connected to the input comparator.

Thanks!

Edit Notes

fix name of pin in title
[edited by: binuggi at 7:52 PM (GMT -4) on 1 Oct 2026]
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.