Dear ADI team.
I would like to inquire about the output voltage range of the AD8055.
According to the datasheet, the output voltage swing is specified as approximately ±3.9 V to ±4.1 V (typical), depending on the load condition, when operating with a ±5 V supply.
Could you please let us know whether there is a specified maximum output voltage swing value (for example, a guaranteed maximum or limit specification) under these conditions?
Additionally, if the maximum output voltage is not specified, could you please advise on a suitable method or circuit for clamping the output voltage of a high-speed signal line?
We would appreciate any recommendations for minimizing the impact on signal integrity and bandwidth while providing output voltage limiting.
Best regards,
Yoshiba