AD549
Production
The AD549 is a monolithic electrometer operational amplifier with very low input bias current. Input offset voltage and input offset voltage drift are...
Datasheet
AD549 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
ADA4077-1
Recommended for New Designs
The single ADA4077-1, dual ADA4077-2, and quad ADA4077-4
amplifiers feature extremely low offset voltage and drift, and low
input bias current, noise,...
Datasheet
ADA4077-1 on Analog.com
I am trying to do a noise analysis of a discrete JFET input stage, hybrid amplifier using two opamps in the feedback loop, one for setting the DC operating point of the JFET. Using the AD549 model works nicely, but the ADA 4077 or similar, ADA 4620 fails. I tried several different other OpAmps with no success.
Any ideas ?
Hello Lippmann ,
I checked your schem and it seems like the 2nF cap on the feedback of the bottom amp.
Can I know why you need that large cap at the feedback?

Best Regards,
Kenneth
Hello Kenneth, the 2nF is not critical - the circuit works with anything from 10pF upwards but using a somewhat larger Cap will reduce noise that feeds into the front end transistor. However, that was not the question- my problem is that the the noise simulation will not converge with the ADA 4077 or similar but smoothly does so using the AD549 for the bottom amp. Do you have any idea for that? The answer to that question is not so important for my project; I am just beeing curious. Thanks for taking the time to look into this!