Does the OVP work with power off?
ADA4177-2
Recommended for New Designs
The ADA4177-1 single-channel, ADA4177-2 dual-channel, and ADA4177-4 quad-channel amplifiers feature low offset voltage (2 μV typical) and drift (1 μV...
Datasheet
ADA4177-2 on Analog.com
Does the OVP work with power off?
Hello kb2026 ,
Yes. The main purpose of OVP is to prevent damage to the input pins if the signal source, such as a sensor, gets powered up before the op amp does.
You can read this article for ADA4177 OVP: Op Amp Input Overvoltage Protection: Clamping vs. Integrated | Analog Devices
Best Regards,
Kenneth
Hello kb2026 ,
Yes. The main purpose of OVP is to prevent damage to the input pins if the signal source, such as a sensor, gets powered up before the op amp does.
You can read this article for ADA4177 OVP: Op Amp Input Overvoltage Protection: Clamping vs. Integrated | Analog Devices
Best Regards,
Kenneth