| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 63 hours |
MStokowski |
Awaiting Customer Response |
LT6203
Production
The LT6202/LT6203/LT6204 are single/dual/quad low noise, rail-to-rail input and output unity gain stable op amps that feature 1.9nV/√Hz noise voltage...
Datasheet
LT6203 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
LT6020
Recommended for New Designs
The LT6020 is a low power, enhanced slew rate, precision operational amplifier. The proprietary circuit topology of this amplifier gives excellent slew...
Datasheet
LT6020 on Analog.com
I am trying to evaluate the stability of an LT6203 driving a capacitive load in LTspice, but I am not sure if my AC loop-gain testbench is correct.
I attached my current LTspice schematic and AC plot. In this setup, I tried to break the feedback loop and inject an AC source, then plot V(in_m)/V(fb). However, the result does not look meaningful. I suspect my biasing or loop-breaking method is wrong.
I am also not sure how to interpret the datasheet for this load. The datasheet shows overshoot vs capacitive load, but the plots only go up to 1000 pF, while my load is 2 nF with a 20 ohm series resistor. Therefore I cannot tell from the datasheet whether this load should be expected to cause excessive overshoot, ringing, stability problems, or any issue related to driving a high capacitive load.