MAX40263
Production
The MAX40263 is a dual-channel operational amplifier with two channels that can be disabled separately with two individual pins.
The MAX40263 offers...
Datasheet
MAX40263 on Analog.com
MAX74822
Recommended for New Designs
The MAX74822 is a dual rail-to-rail input and output, single-supply amplifier featuring very low supply current and 1MHz bandwidth. All are guaranteed...
Datasheet
MAX74822 on Analog.com
Hi
MAX40263 and MAX74822 seems having protection diode internally from Input Current of Absolute Maximum Ratings.
if my understanding is correct and you have VESD information like HBM, please let me know.
Best regards
Thank you for providing answer.
Thank you for providing answer.