Post Go back to editing

VESD information of MAX40263 and MAX74822

Thread Summary

The user inquired about the VESD HBM for the MAX40263 and MAX74822. The final answer confirmed that the VESD HBM for the MAX74822 is ±2000V, but VESD data for the MAX40263 is not available.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX40263, MAX74822

Hi 

MAX40263 and MAX74822 seems having protection diode internally from Input Current of Absolute Maximum Ratings.

if my understanding is correct and you have VESD information like HBM, please let me know.

Best regards

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.